Re: iMX6UL-EVK: How do I use MFG-TOOL to boot from QSPI Nor Flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: iMX6UL-EVK: How do I use MFG-TOOL to boot from QSPI Nor Flash?

1,026 Views
nitigupta
Contributor I

Hello All,

I am also trying to boot Linux from QSPI and also tried MFG tool to do the same but MFG tool script allows to copy only u-boot to QSPI as well as QSPI header. I want to burn zImage, device tree & root file system also on QSPI but failed to understand how to do partition of QSPI flash.
Is there any tutorial available for the same. Any help is appreciated.

Thanks,
Niti

0 Kudos
Reply
1 Reply

777 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Additionally it may be required to configure  U-boot environment to boot properly kernel.

Please look at section 4.7.4 (Running the Linux OS image from QuadSPI) in “i.MX_Linux_User's_Guide.pdf”.

 

< http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... >

  Also, please look at the following :

https://community.nxp.com/message/491138 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply