Re: eMMC Fuses And Card did not respond to voltage select! I.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: eMMC Fuses And Card did not respond to voltage select! I.MX6UL

751 Views
jochenstehle
Contributor III

Hello Yuri Muhin,

we have a simmilar problem with emmc on our custom board.

We use the seriell Downloader via uart to download uboot. But if we use the mmc dev command to chance to the emmc there is an "Card did not respond to voltage select!" error.

We have no resisters on the CFG Pins. Is it absolutely necessary to have those resistors or burn the fuses to communicate with an eMMC in UBOOT?

Best regards

Jochen

0 Kudos
Reply
1 Reply

545 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  No,is it not absolutely necessary to have those resistors or burn the fuses to communicate with

an eMMC in UBOOT? Fuse only boot configuration may be used. You may create request  / ticket to get

some patches, that may help.

 

Support|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply