Re-burning a fuse register on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re-burning a fuse register on iMX6

641 Views
colinhelliwell
Contributor III

I assume (though I'm not certain) that if a fuse register - e.g. one of the secure boot ones - is written to then 1s cannot be subsequently changed back to 0s.

But if you write 1's in two operations, does it result in an OR of the values?

In other words, does

    fuse prog -y 3 0 0x00000001; fuse prog -y 3 0 0x00000010

give the same result as

    fuse prog -y 3 0 0x00000011

Labels (2)
1 Reply

431 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello colinhelliwell,

That’s correct. As fuses cannot go back from 1 to 0, it would be equivalent to an OR. You should be able to do this on the i.MX6 without problem.

However, this may not be true for other One Time Programmable memories in the market depending on their features.

Regards,

0 Kudos