Ramdisk image is corrupt or invalid

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ramdisk image is corrupt or invalid

3,323件の閲覧回数
秀超田
Contributor I

platform:IMX6Q

In download mode,The following error occurred:

Hit any key to stop autoboot:  0

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-2563-gd970361

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3162980 Bytes =  3 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... Bad Data CRC

ERROR: can't get kernel image!

Hardware where will lead to this error

ラベル(1)
0 件の賞賛
返信
1 返信

1,648件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Seems the kernel is not exist. Please try to program the kernel image (uImage) again. You can use the MFGtool to program the images.

0 件の賞賛
返信