Ramdisk image is corrupt or invalid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ramdisk image is corrupt or invalid

3,345 Views
秀超田
Contributor I

platform:IMX6Q

In download mode,The following error occurred:

Hit any key to stop autoboot:  0

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-2563-gd970361

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3162980 Bytes =  3 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... Bad Data CRC

ERROR: can't get kernel image!

Hardware where will lead to this error

Labels (1)
0 Kudos
Reply
1 Reply

1,670 Views
jimmychan
NXP TechSupport
NXP TechSupport

Seems the kernel is not exist. Please try to program the kernel image (uImage) again. You can use the MFGtool to program the images.

0 Kudos
Reply