RX FIFO ERROR while both camera streaming

cancel
Showing results for 
Search instead for 
Did you mean: 

RX FIFO ERROR while both camera streaming

185 Views
Contributor I

Hi,

I am using the linux kernel 4.14.78 from sumo bsp in imx8m EVK (REV-B4) board. I can able to successfully stream the cameras in both minisas connectors individually. But when i tried to stream the both cameras simultaneously i received the RX_FIFO_OVERFLOW error. In NXP release notes they already mentioned about this issue i also attached the screenshot here for your referance. so, Is there any workaround for this issue.

When did you planned to deliver the next release?

Thanks

vimal.

0 Kudos
2 Replies

48 Views
NXP Employee
NXP Employee

Hello,

Unfortunately, we do not have that type of information. I apologize for the inconveniences this could you.

Best regards,

Diego.

0 Kudos

48 Views
Contributor I

Hi Diego Adrian Cuevas

I need to use both the cameras simultaneously, but when i tried to do the same i faced this RX_FIFO_OVERFLOW error from one of the camera very frequently. How to solve this issue? Any comments would really helpful for us.

Thanks,

Vimal.

0 Kudos