RTC issue in latest bsp imx-5.4.24-2.1.0.xml

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC issue in latest bsp imx-5.4.24-2.1.0.xml

Jump to solution
940 Views
rakesh_patel
Senior Contributor I

Board

=======

imx6sx

 

Issue logs

===========

root@imx6sxsabresd:~# date
Sat Sep 26 07:01:42 UTC 2020
root@imx6sxsabresd:~# hwclock
Thu Jan 1 00:01:47 1970 0.000000 seconds

Issue

==========

1) older BSP(imx-4.1-krogoth) have following scripts to manage RTC:

init.d/save-rtc.sh init.d/hwclock.sh init.d/bootmisc.sh

 

But, the above files not there on the new BSP release. So, it looks like RTC not working.

 

Query

==========

1) Is there any replacement script/binaries for the same?

 

Labels (1)
0 Kudos
Reply
1 Solution
933 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply
2 Replies
924 Views
rakesh_patel
Senior Contributor I

Thanks for your reply. New filesystem have NTP as default. So hwclock sync was creating the issue.

0 Kudos
Reply
934 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply