RTC in the iMX537 cpu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC in the iMX537 cpu

3,451件の閲覧回数
jomeke
Contributor II

Hi all,

we developed a custom board with the iMX537 and the PMIC MC34708 chip.

On the PMIC, there is a coin cell connected (3V CR2032) on the LICELL pin.

If we program the RTC on the CPU, the RTC runs perfect until we cut the power, afterwards, all the RTC registers are reset.

We have tried the same on a (changed) QSBoard and have the same behavior.

While the power is cut, the voltage VSRTS drops from 1.3V to 1.23V and the 32Khz clock keeps running.

Is there anbody who has already successfull used the iMX537 RTC function, so yes can you give me any sugestion where to look for ?

Best regards

Johan

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,765件の閲覧回数
jomeke
Contributor II

This is the answer that we received from Freescale :

In reply to your Service Request SR 1-894779544:

OK, Got it. Some customers also met the same problem. I just now adjusted power up sequence. Do it like this :
VDD_DIG_PLL(1.3v) supplies for VDDA and 1V3_VGEN1 supplies for VDDAL, SRTC can be kept after cold reset. So please retry it !

0 件の賞賛
返信

2,765件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please refer to ENGcm12374 (SRTC loses data while powering up/down)

from the Errata.

http://cache.freescale.com/files/32bit/doc/errata/IMX53CE.pdf

Regards,

Yuri.

0 件の賞賛
返信

2,765件の閲覧回数
Gokul
Contributor I

in which file we need to change this??

0 件の賞賛
返信

2,765件の閲覧回数
JohnGoodman
Contributor I

How did you program your RTC and which RTC did you program? 

Did you program the RTC on the PMIC or the SRTC on the i.MX537?

If you are using Linux, RTC0 will be the processor SRTC and RTC1 will be the PMIC RTC.  You will want to use the PMIC RTC ( RTC1 ) for your coin cell backed up RTC.

0 件の賞賛
返信

2,765件の閲覧回数
marek1z
Contributor I

Hi Johan,

We use the iMX535 and have a similar (probably the same) issue - I assume we are dealing with the same problem.

First, look at the Errata sheet for your processor. For the iMX535, errata #23 identifies this exact problem. The workaround is to connect an additional circuit to VDDLP pin on the PMIC (shown in errata sheet), however, when we have done that we experienced a rapid battery drain - we are currently investigating how to solve this problem.

0 件の賞賛
返信