RTC alarm wakeup from shutdown

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTC alarm wakeup from shutdown

1,561 次查看
pratyushtomar
Contributor IV

We have a custom board with i.MX6UL processor. We are using ATWILC3000 wifi module (SPI interface) ATWILC3000 - Wireless Modules  on our board. The RTC alarm wake up from shutdown works fine if don't enable wifi module. But the main problem is that wake up from shutdown by RTC alarm is unreliable if we enable wifi module. Even if we disable wifi module just before shutdown wake up from shutdown doesn't work. I haven't been able to make any correlation between wifi module and RTC alarm wake up from shutdown. Any suggestion for resolving the problem. 

We are using Linux kernel 4.1.

标签 (3)
标记 (1)
0 项奖励
回复
1 回复

1,306 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pratyush

one can try with unit test (imx-test../rtcwakeup.c)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz
One can pay attention that when processor was powered off, wifi module

also was powered off, to avoid parasitic leakage to unpowered processor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复