RTC_XTALI input Voltage of i.MX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC_XTALI input Voltage of i.MX6UL

517件の閲覧回数
T_Abe
Contributor I

Dear Community,
I have a question about the i.MX6UL.

Question
1.Please tell me how many 〇us after VDD_SNVS_CAP (1.1V) is output after VDD_SNVS_IN (3.3V) is input.
2.Do Limitations 1 and 2 below not need to be considered in a transient state?
(When an external 1.0V voltage is input to XTALI at the same time as VDD_SNVS_IN)

Conditions
1.VDD_HIGH_IN and VDD_SNVS_IN are shorted, and this 3.3V power source has a margin of current that can be passed.
2. No load is connected to VDD_SNVS_CAP.
3.No button battery
4.BOOT MODE [1:0] = 1:0 (internal boot) using QSPI

Background
We input an external 32kHz clock to XTALI (T16).
However, there are three limitations listed in the Hardware Development Guide (HDL):

Limitation
1.HDG_P13 RTC_XTALI should not exceed the voltage value of VDD_SNVS_CAP (approximately 1.1V).
2.HDG_P13 The RTC_XTALI signal should not be driven if the VDD_SNVS_CAP supply is off.
3.HDG_P11 Do not connect any loads to VDD_SNVS_CAP.

Solution
1.Set the upper voltage limit of the clock signal to an external power supply of 1.1V or less.
2.External power supplies less than 1.1V should be started after VDD_SNVS_CAP.
3.No load is connected to VDD_SNVS_CAP.

Best Regards.

ラベル(2)
0 件の賞賛
返信
0 返答(返信)