Hi,
I have a RTC application which sets the time using RTC_SET_TIME ioctl call. After executing the app, the time is being set and I am reading it using RTC_RD_TIME which is working fine. But once the date is set and if I do a soft reboot of the board, next time if I read the date , it is showing an old value. But after a hard reboot the updated value is being displayed.
I tried soft reboot after setting the date through command line using date -s and hwlock -w comands. In this case also date is being updated without any issue. I tried an ioctl flush and a system call of hwclock -w from the app after the RTC_SET_TIME ioctl but the value are not being retained after soft reboot.
What is actually happening here?. Can anyone explain.?
@anjalikkrishna
There is general recommendation do not use software reset for i.MX
devices; total system POR should be performed in order to avoid issues
with unpredictable states of external devices.
~Yuri.