RTC Cystal for i.MX6 Dualite System

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC Cystal for i.MX6 Dualite System

689 Views
krishnaprasada
Contributor I

Hi,

I am using i.MX6 Dualite for one of my design.

The system is turned ON by connecting a switch to the ON_OFF Button of the processor.

What would the impact of not using RTC Crystal in my System in this scenario?

Whether the system Can generate PMIC_ON_REQ signal without 32KHz clock? Note that VDD_SNVS_IN supply is still present in the system.

Thanks and Best Regards,

KP

0 Kudos
Reply
1 Reply

427 Views
Yuri
NXP Employee
NXP Employee

   According to section 60.5 (Power-On Reset and power sequencing) of the

i.MX6(Q) Reference Manual : "The 4ms and 1ms delays are derived from counting the

32kHz RTC clock cycles; the accuracy depends on the accuracy of the RTC. When the

RTC crystal is either absent or in the process of powering up, an internal ring oscillator

will be the source of RTC." So, external RTC clock is not needed for start up.

0 Kudos
Reply