RTC Cystal for i.MX6 Dualite System

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTC Cystal for i.MX6 Dualite System

648 次查看
krishnaprasada
Contributor I

Hi,

I am using i.MX6 Dualite for one of my design.

The system is turned ON by connecting a switch to the ON_OFF Button of the processor.

What would the impact of not using RTC Crystal in my System in this scenario?

Whether the system Can generate PMIC_ON_REQ signal without 32KHz clock? Note that VDD_SNVS_IN supply is still present in the system.

Thanks and Best Regards,

KP

0 项奖励
回复
1 回复

386 次查看
Yuri
NXP Employee
NXP Employee

   According to section 60.5 (Power-On Reset and power sequencing) of the

i.MX6(Q) Reference Manual : "The 4ms and 1ms delays are derived from counting the

32kHz RTC clock cycles; the accuracy depends on the accuracy of the RTC. When the

RTC crystal is either absent or in the process of powering up, an internal ring oscillator

will be the source of RTC." So, external RTC clock is not needed for start up.

0 项奖励
回复