各位好:
现在在进行#RT1176CVM8A设计,有两个设计问题,还请大神赐教:
基本需求:2路千兆网,NOR FLASH启动,2片16位的s DRAM组成32位接口
1. 启动问题。
由于我需要出两路千兆网,选择了SD2和DISP_B1的RGMII接口,导致无法使用原先的FlexSPI A(SD_B2)。我想选用sd_b1(FlexSPI2 Secondary pin Group)作为系统默认启动的NOR FLASH接口,除了BOOT_CFG[11]选择FlexSPI2之外,是否必须要进行eFuse烧写配置?
2.RGMII接口选择问题。
如上图所示,选择两路千兆网口,ENET_1G和ENET_QoS,这样选择是否可以?规格书里理解的不是很确定。
谢谢您的宝贵时间!
Hi,
感谢回复。
1)eFuse烧写配置我注意到是通过MCUBOOTUTILITY进行的,在批量生产时需要产线工人输入配置值进行烧录,然后再烧录固件。因为efuse是一次性的,这样风险比较大。请问有没有好的办法能将风险减小,或将efuse烧录和flash烧录合并成一次?
-- 对于MCUBOOTUTILITY,它是利用flashload和 Serial Download模式来烧写代码,同时flashload也可以烧写eFuse,所以针对大批量生产,最好是写一个脚本既能烧录代码又能烧录eFuse.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
1) 除了BOOT_CFG[11]选择FlexSPI2之外,是否必须要进行eFuse烧写配置?
-- 需要将FLEXSPI_PIN_GROUP_SET fuse bit置1。
2)选择两路千兆网口,ENET_1G和ENET_QoS,这样选择是否可以?
-- 可以。
3)你的选择从FlexSPI2的 Secondary pin Group连接的QSPI flash启动没问题,但是Secondary pin Group没有DQS脚,所以只能工作在低速,所以我建议使用Hyper RAM替代SDRAM, 从而可以选择其他FlexSPI脚连接QSPI flash.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
您好,
非常感谢您的回答!
还有一些问题:
1. eFuse烧写配置我注意到是通过MCUBOOTUTILITY进行的,在批量生产时需要产线工人输入配置值进行烧录,然后再烧录固件。因为efuse是一次性的,这样风险比较大。请问有没有好的办法能将风险减小,或将efuse烧录和flash烧录合并成一次?