RT1176 firmware downloading via Ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1176 firmware downloading via Ethernet

761件の閲覧回数
JayCao
Contributor III

Hello,

We are building a system that needs to download the firmware via Ethernet (not OTA).

Could you share with us any guides or examples to help us build this system?

Thanks and BRs,

ラベル(2)
0 件の賞賛
返信
1 返信

749件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @JayCao ,

RT1176 boot ROM doesn't support ENET. So at least there must be a bootloader which can access ENET and an application.

You can refer to the opensource bootloader demo in SDK or the SBL&SFW project.

These two example are real OTA. I don't know how to download application to system by ENET without OTA.

Maybe you can have something like a debug probe which can download code from ENET and download to RT1176 via UART/USB/JTAG?

 

Regards,

Jing

0 件の賞賛
返信