RT1176 JTAG_MOD pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 JTAG_MOD pin

793 Views
karaca
Contributor I

Hi,

 

We designed a custom board with IMXRT1176. We connected to board all JTAG pins. But JTAG_MOD pin is float. We can not make JTAG connection. What can you suggested us?

0 Kudos
5 Replies

766 Views
karaca
Contributor I

Hi Omar,

Thanks for your information. JTAG_MOD is float in our hardware. Can we change JTAG_MOD pin to float with software? We can use USB and UART communications but we need JTAG.

 

Thanks.

0 Kudos

762 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Unfortunately, JTAG_MOD needs to be externally connected to GND so JTAG works correctly. 

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos

755 Views
karaca
Contributor I

Hi Omar,

 

We connected JTAG_MOD pin to GND with rework. But we still can not connect JTAG. Our connection in below.

 

karaca_0-1663741931538.png

 

Do you have any suggestion? 

Thanks. Regards.

0 Kudos

747 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

It is important that you´ve followed the recommendations from the Hardware Development Guide. External resistors can be used with all JTAG signals except for JTAG_TDO, but they are not required.
Did you burn any fuse?

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos

772 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

When JTAG_MOD is low, the JTAG interface is configured for a common software debug, adding all the system TAPs to the chain.
When JTAG_MOD is high, the JTAG interface is configured to a mode compliant with the IEEE 1149.1 standard.
JTAG_MOD shall be externally connected to GND for normal operation in a system. The termination to GND through an external pull-down resistor is allowed using a 4.7-kΩ resistor.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos