RT1176 DMA major IRQ too often

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 DMA major IRQ too often

747 Views
NXPur
Contributor I

I want to read from LPSPI1 a 4 byte value from RDR twice => 8 bytes in a ring buffer  via DMA with major end irq like this:  (LPSPI fifo watermarks are zero)

DMA0->TCD[0].SADDR = (uint32_t) &LPSPI1->RDR;
DMA0->TCD[0].DADDR = (uint32_t) slaveRxData;
DMA0->TCD[0].ATTR = 0x0202; // SSIZE=2 DSIZE=2
DMA0->TCD[0].SOFF = 0;
DMA0->TCD[0].DOFF = 4;
DMA0->TCD[0].NBYTES_MLNO = 4;
DMA0->TCD[0].SLAST = 0;
DMA0->TCD[0].CITER_ELINKNO = 2;
DMA0->TCD[0].BITER_ELINKNO = 2;
DMA0->TCD[0].DLAST_SGA = (uint32_t) ptrRXTCD;
DMA0->TCD[0].CSR = 0x0013; // ESG DREQ INTREQ !!! irq function !!!

but the DMA irq comes after 4 bytes transferred. I want every 8 bytes the irq.

Tags (1)
0 Kudos
Reply
1 Reply

736 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @NXPur,

I believe you should take a look into the EDMA_PrepareTransfer() function from the edma. This function includes the parameter “transferBytes” and “bytesEachRequest”, which dictate the amount of bytes that will be transfer every minor and major loop of the DMA request, before executing the IRQ. Please let me know if this helps.

 

BR,

Edwin.

0 Kudos
Reply