RT1172 MCU Config Tools Support for SEMC SRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1172 MCU Config Tools Support for SEMC SRAM

Jump to solution
1,731 Views
mjosborne1
Contributor III

Hello,

I'm trying to configure the RT1172 SEMC for SRAM using MCUXpresso Config Tools Version 13.1.

I only see SDRAM as an option:

mjosborne1_0-1685482218132.png

There is a reply (2022-08-30) in a similar post here that this will be available via a "Mode" setting in the next release:
https://community.nxp.com/t5/i-MX-Processors/IMXRT1064-How-to-use-and-configure-SRAM-with-SEMC/m-p/1... 

mjosborne1_1-1685482328359.png

Is there a status update on the availability of this feature?

Thank you

0 Kudos
Reply
1 Solution
1,637 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Unfortunately, this is not possible. You might want to copy some parts of the generated code so it can attach to any SDRAM/SRAM mex file. 

Best regards,
Omar

View solution in original post

0 Kudos
Reply
3 Replies
1,675 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

This feature is available in the standalone version of Config Tool, you need to make sure that SEMC is at "register initialization".

Omar_Anguiano_0-1685564103523.png

Best regards,
Omar

 

0 Kudos
Reply
1,665 Views
mjosborne1
Contributor III

Thanks for the info, I see the option now.

Is it possible to define both an SDRAM and SRAM SEMC configuration in the same .mex file?

When I try to add an additional Register Initialization component (already had an SEMC peripheral SDRAM config), or two components - one for each of SDRAM and SRAM - I get an error about the peripheral being used in multiple instances.

Best regards,

Matt

0 Kudos
Reply
1,638 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Unfortunately, this is not possible. You might want to copy some parts of the generated code so it can attach to any SDRAM/SRAM mex file. 

Best regards,
Omar

0 Kudos
Reply