RT1064-Some questions about sdphost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1064-Some questions about sdphost

ソリューションへジャンプ
1,611件の閲覧回数
Alexander-cloud
Contributor I

I use the RT1064EVK board, I first download the spi_nor routine of the gpio of the SDK to the board, and then adjust the switch to make the board work in the serial download mode, I use the sdphost host computer, and use the jump command to make the board run prepared in advance Flashing light program, but I can't implement it, here are some pictures

jump.png

0 件の賞賛
返信
1 解決策
1,595件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In my opinion, it's impossible to jump the code in the flash via the jump-address command, further, the FlexSPI needs to be configured to access via the AHB bus prior to jump operation, definitely, the jump-address command can't support the feature.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,596件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In my opinion, it's impossible to jump the code in the flash via the jump-address command, further, the FlexSPI needs to be configured to access via the AHB bus prior to jump operation, definitely, the jump-address command can't support the feature.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------

0 件の賞賛
返信