Hi Omar,
Thank you.
Here is what I tested, can you tell where I am wrong?
I trying to test RT1064-EVK and have the following issues:
I am using P&E multilink universal to program LED demo application to RT1064-EVK
1) If I use J21(20Pin connector) and remove J47, J48, I can program FlexSPI flash and run properly.
2) If I use J34(10Pin connector) and remove J47, J48, I can't program FlexSPI flash and got the following error
"pegdbserver_console.exe" stop working.....
Can anybody help me to fix this issue?
Thanks,
Christie