RT1052 sd卡读取很慢

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052 sd卡读取很慢

1,074 Views
InvisibleWind
Contributor I

您好,我在使用RT1052的USDH1外设操作sd卡的时候,发现USDH读取和写入sd卡block时间太长的问题,我使用的sdk版本是SDK_2_13_0,用的是sdmmc_examples/sdcard_fatfs_freertos,配置sd时钟为198MHz,sd卡正确识别为SDR104,并且fatfs文件操作均正常,示波器观察clk确实是198MHz

qingfeng_0-1694172318759.png

但是底层函数sd卡读取和写block时间太长了,理论读取两个block(512byte*2)为1024byte,在四线情况下,需要2048个时钟,198MHz情况下,理论上需要时间为1/198*2048=10.3us,但是实际操作两个block时间为3.87ms(链接脚本中,代码运行在SDRAM和Nor Qspi Flash我都尝试了,问题一样)

SDS5104X_PNG_1.png

 这严重超出正常预期,block读写时间过长导致我的上层FATFS读写1M的文件都需要1到2秒时间,SD卡的高速读写能力对项目至关重要,并且我认为带SD3.0外设性能强悍的RT系列不应该是这个速度,我想知道这种问题可能出现的原因是什么,该如何解决。

附:

我的系统时钟配置如下

 
 

HFQK@[E~7NU0]_)IXNK9CX7.png

 我几乎没修改SDK中sdmmc_examples/sdcard_fatfs_freertos的代码

我能确认测试过程比较严谨

应用重要代码

X(A@ORBD1}~XS@$_L[N@QIT.png

 底层打标记

EU8I0IT{9MQ{5PS$JS1)PH5.png

 串口输出的连续的block读写打印信息

R2OQ}B`}WKM[2[PS6J0EUGD.png

然后就是上面示波器的CLK波形,一块一块的出现在示波器上面,并且时间我用光标指示出来了

 

Best wishes

 

 

 

 

 

 

 

 

 
 

 

0 Kudos
Reply
2 Replies

1,007 Views
vicentegomez
NXP TechSupport
NXP TechSupport

would be possible that you put your question in English 

 

regards

 

0 Kudos
Reply

1,005 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I saw your other thread

 

0 Kudos
Reply