RT1021 SDP response 0x89232389 meaning?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1021 SDP response 0x89232389 meaning?

565件の閲覧回数
rshipman
Contributor V

Hi,

What does the SDP response 0x89232389 mean please?

It looks like a valid response, but I could not find documentation for it. My guess it means something like either 'bad number argument' or 'illegal address'.

I know about these responses:

0x128A8A12      WRITE_REGISTER - WRITE_COMPLETE
0x88888888      WRITE_FILE - WRITE_COMPLETE
0x12828212 or 0x128A8A12*     DCD_WRITE - WRITE_COMPLETE
0x33333333      HAB Failure
0x69696969      HAB Warning
0xf0f0f0f0      HAB Success

0x89232389      Unknown!

And then there are the security config responses:

0x12343412      HAB Closed
0x56787856      HAB Open

Is there a complete definitive list of all the possible SDP responses please?

*In the section 9.9.2.1.5 DCD_WRITE, the text says the response should be 0x12828212 but the description of Report 4 suggests it should be 0x128A8A12 (same as WRITE_REGISTER - WRITE_COMPLETE). I haven't checked this, it would be good if you could confirm what the response should be for DCD_WRITE.

Many thanks,

Ronnie

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

556件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there a complete definitive list of all the possible SDP responses, please?
-- No, there's no such a file.
2) What does the SDP response 0x89232389 mean please?
-- From my experience, I was wondering if you can introduce the testing steps of replicating the response value firstly.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信