RS485 tx/rx gpio pin control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RS485 tx/rx gpio pin control

1,867件の閲覧回数
pawe_rogo_
Contributor I

Hi,

The RS485 communication work on my board with imx233 but to transmit or receive I have to control manually by GPIO (pin set 1 - TX, set 0 - RX). Where can I add to DUART driver some line to set the gpio before transmit and reverie?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,292件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

which bsp are you using?

0 件の賞賛
返信

1,292件の閲覧回数
pawe_rogo_
Contributor I

What is the bsp? :smileyhappy:

I use Linux kernel 3.13-rc4 on imx233 (own board).

Oh that is my old thread :smileygrin:. I wrote that when I try do it on old kernel. Now in new kernel I want to do it by modify the mxs-auart.c file.

0 件の賞賛
返信