RS232 and USB detection is not happening at host side with imx6ull device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RS232 and USB detection is not happening at host side with imx6ull device

382 次查看
LoKi
Contributor II

I am trying to upgrade kernel from Linux kernel v4.1.15 to Linux kernel v6.6.36 for IMX6ULL ultralite. After upgrading Linux kernel with v6.6.36, RS232 and USB detection is not happening at host side while I am using u-boot version 2017.03.

Can anyone suggest what is wrong and in which direction I need to debug?

0 项奖励
回复
2 回复数

350 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Please share the complete log of the issue in .txt format of the old and the new version.

You are working with an old u-boot (2017), Is recommended to upgrade to U-Boot v2024.04, if you have an EVK you can test it with the BSP in https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for...

 

0 项奖励
回复

376 次查看
LoKi
Contributor II

Device side RS232 and USB cable is able to identified.

0 项奖励
回复