RS232 and USB detection is not happening at host side with imx6ull device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RS232 and USB detection is not happening at host side with imx6ull device

370件の閲覧回数
LoKi
Contributor II

I am trying to upgrade kernel from Linux kernel v4.1.15 to Linux kernel v6.6.36 for IMX6ULL ultralite. After upgrading Linux kernel with v6.6.36, RS232 and USB detection is not happening at host side while I am using u-boot version 2017.03.

Can anyone suggest what is wrong and in which direction I need to debug?

0 件の賞賛
返信
2 返答(返信)

338件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Please share the complete log of the issue in .txt format of the old and the new version.

You are working with an old u-boot (2017), Is recommended to upgrade to U-Boot v2024.04, if you have an EVK you can test it with the BSP in https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for...

 

0 件の賞賛
返信

364件の閲覧回数
LoKi
Contributor II

Device side RS232 and USB cable is able to identified.

0 件の賞賛
返信