RS232 and USB detection is not happening at host side with imx6ull device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RS232 and USB detection is not happening at host side with imx6ull device

249 Views
LoKi
Contributor II

I am trying to upgrade kernel from Linux kernel v4.1.15 to Linux kernel v6.6.36 for IMX6ULL ultralite. After upgrading Linux kernel with v6.6.36, RS232 and USB detection is not happening at host side while I am using u-boot version 2017.03.

Can anyone suggest what is wrong and in which direction I need to debug?

0 Kudos
Reply
2 Replies

217 Views
Oswalag
NXP TechSupport
NXP TechSupport

Please share the complete log of the issue in .txt format of the old and the new version.

You are working with an old u-boot (2017), Is recommended to upgrade to U-Boot v2024.04, if you have an EVK you can test it with the BSP in https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for...

 

0 Kudos
Reply

243 Views
LoKi
Contributor II

Device side RS232 and USB cable is able to identified.

0 Kudos
Reply