RPMsg performance Benchmark

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RPMsg performance Benchmark

Jump to solution
6,062 Views
jithesh77
Contributor I

Hi

RPMsg communication performance Benchmark is available for i.Mx8QXPlus between Cortex-A35 and M4 Cores .What will be the maximum communication speed we can achieve ?.

Thanks

Jithesh

0 Kudos
Reply
1 Solution
5,995 Views
joanxie
NXP TechSupport
NXP TechSupport

I attached the test result which is based on i.MX8QXP C0 MEK board REV D4 with L5.4.3_2..0.0, hope helpful for you

 

 

 

View solution in original post

0 Kudos
Reply
5 Replies
5,985 Views
jithesh77
Contributor I

Hi,

Thanks for the support and Test results.

Thanks

Jithesh

0 Kudos
Reply
6,041 Views
jithesh77
Contributor I

Hi 

Could you please confirm on the RPMsg performance if somebody is familiar with RPMsg between Cortex-A35 and M4 Cores in i.Mx8QXPlus

Thanks in Advance

Jithesh

0 Kudos
Reply
5,996 Views
joanxie
NXP TechSupport
NXP TechSupport

I attached the test result which is based on i.MX8QXP C0 MEK board REV D4 with L5.4.3_2..0.0, hope helpful for you

 

 

 

0 Kudos
Reply
4,244 Views
Majidbahmani
Contributor II

Hi,

I would like to test RPMsg performance between Cortext-A53 and Cortex-M7 for IMX8M Plus. Is there any similar "RPMsg Performance Benchmark" for IMX8M Plus?

Thank you.

 

2,662 Views
VishalGSawarkar
Contributor I
Its good to see that you took this test. If you have any data. Can you post here?
0 Kudos
Reply