Hello,
We have custom modules based on imx6sx.
Our firmware based on Yocto Project Version 2.5 (sumo) - everythig works fine of it.
Last time we updated Yocto to versio 2.7 (warrior), but Ethernet doesn't work on it.
So kernel was updated from 4.1 to 4.9 (we tested also 4.19).
We use RMII mode (50Mhz + SION bit is set).
So when SION bit is set (according to description in imx6sx-pinfunc.h) the kernel (v4.9) hang on Network configuration.
What could possibly be wrong?
Here you have part of our dts file:
#include "imx6sx.dtsi"
...
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet1>;
phy-reset-gpios = <&gpio2 0 0>;
phy-mode = "rmii";
status = "okay";
};
...
pinctrl_enet1: enet1grp {
fsl,pins = <
MX6SX_PAD_ENET1_MDIO__ENET1_MDIO 0x1b0b1
MX6SX_PAD_ENET1_MDC__ENET1_MDC 0x1b0b1
MX6SX_PAD_RGMII1_RX_CTL__ENET1_RX_EN 0x1b0b1
MX6SX_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x0051
MX6SX_PAD_RGMII1_TD0__ENET1_TX_DATA_0 0x1b0b1
MX6SX_PAD_RGMII1_TD1__ENET1_TX_DATA_1 0x1b0b1
MX6SX_PAD_RGMII1_TX_CTL__ENET1_TX_EN 0x1b0b1
MX6SX_PAD_RGMII1_RD0__ENET1_RX_DATA_0 0x1b0b1
MX6SX_PAD_RGMII1_RD1__ENET1_RX_DATA_1 0x1b0b1
MX6SX_PAD_ENET1_COL__GPIO2_IO_0 0x10b0
>;
};
Here you have part of our patches:
Index: kernel-source/include/linux/mfd/syscon/imx6q-iomuxc-gpr.h
===================================================================
--- kernel-source.orig/include/linux/mfd/syscon/imx6q-iomuxc-gpr.h
+++ kernel-source/include/linux/mfd/syscon/imx6q-iomuxc-gpr.h
@@ -424,9 +424,9 @@
#define IMX6SX_GPR1_VADC_SW_RST_MASK (0x1 << 19)
#define IMX6SX_GPR1_VADC_SW_RST_RESET (0x1 << 19)
#define IMX6SX_GPR1_VADC_SW_RST_RELEASE (0x0 << 19)
-#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK (0x3 << 13)
-#define IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK (0x3 << 17)
-#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_EXT (0x3 << 13)
+#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK (0x1 << 13)
+#define IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK (0x1 << 17)
+#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_EXT (0x1 << 13)
#define IMX6SX_GPR4_FEC_ENET1_STOP_REQ (0x1 << 3)
#define IMX6SX_GPR4_FEC_ENET2_STOP_REQ (0x1 << 4)
Index: kernel-source/arch/arm/mach-imx/mach-imx6sx.c
===================================================================
--- kernel-source.orig/arch/arm/mach-imx/mach-imx6sx.c
+++ kernel-source/arch/arm/mach-imx/mach-imx6sx.c
@@ -84,7 +84,7 @@ static void __init imx6sx_enet_clk_sel(v
regmap_update_bits(gpr, IOMUXC_GPR1,
IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK, 0);
regmap_update_bits(gpr, IOMUXC_GPR1,
- IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK, 0);
+ IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK, IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK);
} else {
pr_err("failed to find fsl,imx6sx-iomux-gpr regmap\n");
}
Index: kernel-source/arch/arm/boot/dts/imx6sx-pinfunc.h
===================================================================
--- kernel-source.orig/arch/arm/boot/dts/imx6sx-pinfunc.h
+++ kernel-source/arch/arm/boot/dts/imx6sx-pinfunc.h
@@ -330,7 +330,7 @@
* also connected to that pin and using respective function as input (e.g.
* UART1's DTR handling on MX6SX_PAD_ENET1_TX_CLK__UART1_DTR_B).
*/
-#define MX6SX_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x0090 0x03D8 0x0760 0x1 0x1
+#define MX6SX_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x0090 0x03D8 0x0760 0x11 0x1
#define MX6SX_PAD_ENET1_TX_CLK__AUDMUX_AUD4_RXD 0x0090 0x03D8 0x0644 0x2 0x1
#define MX6SX_PAD_ENET1_TX_CLK__UART1_DTR_B 0x0090 0x03D8 0x0000 0x3 0x0
#define MX6SX_PAD_ENET1_TX_CLK__SPDIF_SR_CLK 0x0090 0x03D8 0x0000 0x4 0x0
Index: kernel-source/arch/arm/mach-imx/clk-imx6sx.c
===================================================================
--- kernel-source.orig/drivers/clk/imx/imx/clk-imx6sx.c
+++ kernel-source/drivers/clk/imx/clk-imx6sx.c
@@ -617,8 +617,8 @@ static void __init imx6sx_clocks_init(st
imx_clk_set_parent(clks[IMX6SX_CLK_ENET_PRE_SEL], clks[IMX6SX_CLK_PLL2_PFD2]);
imx_clk_set_parent(clks[IMX6SX_CLK_ENET_SEL], clks[IMX6SX_CLK_ENET_PODF]);
imx_clk_set_rate(clks[IMX6SX_CLK_ENET_PODF], 200000000);
- imx_clk_set_rate(clks[IMX6SX_CLK_ENET_REF], 125000000);
- imx_clk_set_rate(clks[IMX6SX_CLK_ENET2_REF], 125000000);
+ imx_clk_set_rate(clks[IMX6SX_CLK_ENET_REF], 50000000);
+ imx_clk_set_rate(clks[IMX6SX_CLK_ENET2_REF], 50000000);
/* Audio clocks */
imx_clk_set_rate(clks[IMX6SX_CLK_PLL4_AUDIO_DIV], 393216000);
Hi Tomasz
nxp does not support yocto version 2.7 (warrior) yet according to
oficial linux documentation (Release Notes sec.2.1 New features) from link
4.19 is based on version 2.6 Thud: Documentation.
One can try with nxp linux from source.codeaurora.org/external/imx repository
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your quick response.
Sorry, I think I wasn't too precise with my description,
we already tested several options.
Our firmware is based on Yocto 2.5, but we didn't update recipes for long time,
so until now our firmware used meta-freescale/recipes-kernel/linux/linux-fslc-imx_4.1-2.0.x.bb for kernel
Today I updated meta-freescale to the newest commit on Sumo branch
so now we have:
linux-fslc-imx_4.9-1.0.x.bb
Unfortunately after rebuild firmware with the new kernel (4.9) the result is the same as for Thud and Warrior - kernel hangs on Configuring network interfaces
here is the end of the kernel log:
mount sdcard
FAT-fs (mmcblk3p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
INIT: Entering runlevel: 5
Configuring network interfaces...
the only things I did after the meta-freescale update were:
* Prepare defconfig for new kernel
* Adjust our patches to meet changes in sources (patches that I described before)
Any idea why it works fine on 4.1 but not on 4.9?
"linux-fslc-imx" is community version of linux not supported by nxp, one can check
difference between Yocto Community BSP and Freescale BSP Release
Please try official nxp linux from source.codeaurora.org/external/imx repository,
follow documentation from i.MX Software | NXP
Best regards
igor
One more thing
we noticed that the clock is not generated
one can start to investigate it in uboot setup_fec() :
mx6sxsabresd.c\mx6sxsabresd\freescale\board - uboot-imx - i.MX U-Boot
We tried official nxp linux (v. 4.9.88),
unfortunately with the same result.