I have a custom board with a imx93 processor (SiliconRev2.0) where we have connected a PHY in RMII mode where the imx93 shall generate a 50MHz clock at MX93_PAD_ENET2_TD2__ENET1_TX_CLK.
The problem is that there are no clock output at all.
We have followed AN14149 'Ethernet Controller Configuration on i.MX 8MP and i.MX 93 Processors' (Rev. 1 — 8 January 2024) chapter 4.3.1 'ENET FEC interface configuration => RMII mode'
Can there be issues related to the new silicon or may there be issues missed out in the application note?
I am reaching out to the forum to get any information that can help us progress in this issue.
Attached follows patched version of fec_main.c with some extra printouts that shows that the code actually to the line where CLK_SEL is written.
Hi,
Thank you for your interest in NXP Semiconductor products,
Seems like the changes from App Note are applied,
Could you confirmed if you probed the ENET2_TD2 pad and saw no clock output at all?
Regards
Yes I measured with oscilloscope at two boards, and there were 0V and no activity.
Hi,
Ok, let me review it.
Regards