RMII clock pin input in, external PHY to MAC, imx8mm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RMII clock pin input in, external PHY to MAC, imx8mm

3,316 Views
triedgetech
Contributor III

I'm using imx8mm (PICO PI imx8mm) on my own board. My PHY is KSZ8091, which works in RMII standard.

PHY generates 50Mhz clock on its ref_clk (by doubling 25Mhz clock from its XO pin I guess) pin:

Screenshot_20220325_154601(1).jpg

In this other thread, someone was trying to do the same, but on imx6.

However, the pad values at node pinctrl_enet2: enet2grp would be different for me.

How different would it be?

I'd need to change my dts file here:

ubuntu-tn-imx/output/kernel/linux-tn-imx/arch/arm64/boot/dts/freescale/imx8mm-pico.dtsi

 

 

 

 

&fec1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_fec1>;
	phy-mode = "rmii";
	phy-handle = <&ethphy0>;
	fsl,magic-packet;
	status = "okay";

	mdio {
		#address-cells = <1>;
		#size-cells = <0>;

		ethphy0: ethernet-phy@0 {
			compatible = "ethernet-phy-ieee802.3-c22";
			reg = <0>;
		};
	};
};
&iomuxc {
	pinctrl-names = "default";

	pinctrl_fec1: fec1grp {
		fsl,pins = <
			MX8MM_IOMUXC_ENET_MDC_ENET1_MDC			0x3
			MX8MM_IOMUXC_ENET_MDIO_ENET1_MDIO		0x3

			MX8MM_IOMUXC_ENET_TD1_ENET1_RGMII_TD1		0x1f
			MX8MM_IOMUXC_ENET_TD0_ENET1_RGMII_TD0		0x1f

			MX8MM_IOMUXC_ENET_RD1_ENET1_RGMII_RD1		0x91
			MX8MM_IOMUXC_ENET_RD0_ENET1_RGMII_RD0		0x91

            MX8MM_IOMUXC_ENET_RXC_ENET1_RX_ER           0x91

			MX8MM_IOMUXC_ENET_RX_CTL_ENET1_RGMII_RX_CTL	0x91
			MX8MM_IOMUXC_ENET_TX_CTL_ENET1_RGMII_TX_CTL	0x1f

			MX8MM_IOMUXC_SD1_RESET_B_GPIO2_IO10	0x19	/* ENET_nRST */
		>;
	};

 

 

 

 

This is what I have currently, and it seems to work. But I'm not convinced this is the right way, for starters, as you can see, there's not even a mention of

MX8MM_IOMUXC_ENET_TD2_ENET1_TX_CLK

Even though the pin, (AG25/ENET_TD2) corresponding to this function, physically connects from MAC side to REF_CLK pin at PHY.

I don't know where is written how MAC side is supposed to receive or send 50Mhz clock in RMII mode, which makes MAC "understand" that TD2 (AG25/ENET_TD2) function is where clock is for RMII, without proper pad configuration in the above mentioned device tree file. If it's "u-boot/u-boot-tn-imx/arch/arm/dts/imx8mm-ddr3l-val.dts", how does it being loaded? How does OS know to load this particular device tree file?

 

Looking at processor manual and by looking at suggestions in this forum, there seems to be IOMUXC_GPR_GPR1 register which has a relevant field called: "GPR_ENET1_TX_CLK_SEL"

I need it to be set to value 0, because RMII clock comes from "external" PHY.

Screenshot_20220325_153903.jpg

Where do I set this value? In imx6, here, a guy edited mach-imx6ul.c, namely:

 

 

 

 

        regmap_update_bits(gpr, IOMUXC_GPR1, IMX6UL_GPR1_ENET2_CLK_DIR,
                   0);
        regmap_update_bits(gpr, IOMUXC_GPR1, IMX6UL_GPR1_ENET2_CLOCK_SEL_MASK,
                   1);

 

 But I have imx8mm, and I couldn't find a relevant file, where is it? Do I make a similar edit?

Labels (1)
0 Kudos
Reply
1 Reply