RIoTboard - Accessing SPDIF input pins
10-09-2014
02:13 AM
630 次查看

NXP Employee
Hi,
we have two RIoTboards in our test setups now, along with other imx6 boards, and they are working great! We are able to use SPI, I2C, UART and other connections. On other boards we now also acitivated the SPDIF input of the imx. Sadly, there is no pin available for this on the RIoT's expansion port.
The possible pins for SPDIF input are:
EIM_DATA_21
ENET_RX_ER
GPIO_16
KEY_COL3
The question is now: How to access one these pins most comfortably?
Does anybody now if GPIO_16 is available on the bottom of the board, so we could solder a wire to it?
Does any of the other pins have an easily accessible contact spot?
Thanks,
Jonas.
0 回复数