RGMII Max Trace Length

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RGMII Max Trace Length

3,392件の閲覧回数
Balaji_ng
Contributor III

Hi,

    I am designing I.MX6SoloX based PCB with dual AR8031 as in Sabre SDB.  The trace lengths of RGMII on my Layout are approximately 5.6 Inch because of the Placement Constraints. However, all the RGMII traces have an unsplit Ground Reference Plane. As per RGMII standards, I understand maximum RGMII trace length is 6 Inches.

In the above context, let me know if the 5.6 Inch is fine.

Regards,

Balaji.V

ラベル(1)
0 件の賞賛
返信
1 返信

2,361件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Balaji

i.MX does not impose additional restrictions on length, so

5.6 Inch would be fine.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------