RESETBMCU pull up resistor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RESETBMCU pull up resistor

Jump to solution
4,138 Views
atillametetured
Contributor V


Hello,

On SPF-27392_C5 page 19 (Sabre for Smart Devices) PMIC Control block, at RESETBMCU is connected directly to POR_B of i.MX6Q. Datasheet for PF0100 says RESETBMCU is an ope-drain output and is asserted low after a turn on event for a given time.

If this is an open drain output which asserts low after a turn on event, shouldnt it be pulled high to VSNVS first and then connected to POR_B?

Best Regards,

Mete

Labels (3)
0 Kudos
Reply
1 Solution
3,728 Views
art
NXP Employee
NXP Employee

The POR_B pad of i.MX6Q has the internal 100kOhm pull-up resistor, that is used here for the reset circuit.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

5 Replies
3,729 Views
art
NXP Employee
NXP Employee

The POR_B pad of i.MX6Q has the internal 100kOhm pull-up resistor, that is used here for the reset circuit.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,728 Views
dharitrihazarik
Contributor I

Hi Artur,

We are using MIPI 10 pin JTAG connector which has only TRST pin and no SRST. How would the system reset occur without SRST and should TRST be connected to POR_B pin of processor for system reset.

Regards,

Dharitri

0 Kudos
Reply
3,728 Views
art
NXP Employee
NXP Employee

The TRST signal is only meant to reset the JTAG state machine, not the whole system. So, without SRST signal, seems that you have to perform the whole system reset manually, as required.

Best Regards,

Artur

0 Kudos
Reply
3,728 Views
dharitrihazarik
Contributor I

Thanks for the response Artur. I have one more doubt.

I am confused with the jtag connector connections;

In lauterbach guide the connections are given as below:

jtag_std_connectors.PNG

But in Sabre (ref schematics), they have connected it as below:

jtag_srst.PNG

Can you please clarify regarding the 9th Pin connection? Does it has to be connected to TRST or should it be grounded?

Thanks,

Dharitri

0 Kudos
Reply
3,728 Views
art
NXP Employee
NXP Employee

If R765 is not populated (as marked on the schematic above), the connector of your JTAG probe can remain unchanged.

Artur

0 Kudos
Reply