RE: Using PICO-IP-iMX7 and Android Things

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RE: Using PICO-IP-iMX7 and Android Things

1,849 次查看
silver2row
Contributor I

Hello,

I have had some difficulty using the iMX7, PICO-IP-iMX7 board, w/ Android Things. I have been unable to use any sort of "Android Things" utilities and I have not been able to connect to the board.

...

Is anyone using this specific board? I wanted to find out how to connect. I tried via Serial and Android Things utility.

I was able to use a couple of commands in a Serial Console for about one session. I could not backspace or set up anything of use. I wanted to try and start using this board.

I keep getting stopped at: Searching for Devices … This can take up to 3 minutes.

After this prompt, my board is inaccessible. 

Seth

P.S. Please reply if you are using this board w/ this OS and software. 

0 项奖励
回复
1 回复

1,597 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The PICO-PI-IMX7 board is from the 3rd party TechNexion, so, you could refer to its product summary page and Support center at the following links:

https://shop.technexion.com/pico-pi-imx7.html

https://www.technexion.com/support/

 

Additionally, maybe marcelvandenheuvel‌ could provide some hints.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------