RE: Request for Support in Adding Features to Yocto Build for imx8qxpc0mek

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RE: Request for Support in Adding Features to Yocto Build for imx8qxpc0mek

1,171 Views
subbuemdtest
Contributor I

Hi @nxp Team,

I have built the Yocto image for the imx8qxpc0mek. Now, I would like to add the following components to my Yocto build. Could you please provide support for this?

  1. How to enable PCIe drivers
  2. Video grabber support
  3. FFmpeg
  4. GStreamer
  5. LVDS to HDMI driver

Your guidance and assistance would be highly appreciated.


Thanks,

Subbu

 

0 Kudos
Reply
5 Replies

1,145 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Most of components should be already included in BSP by default. 

If one of them not included, for example. FFmpeg, hope the layer will be helpful for you OpenEmbedded Layer Index - ffmpeg4

 

Regards

Harvey

0 Kudos
Reply

1,127 Views
subbuemdtest
Contributor I
Hi @Harvey021,

I have got your point. I just want to add these features in my build-
How to enable PCIe drivers
Video grabber support
FFmpeg
GStreamer
LVDS to HDMI driver
Kindly support to enable the features in my image and let me know what changes do I need to change in local.conf file.

Thanks,
Subbu
0 Kudos
Reply

1,115 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @subbuemdtest 

Please refer to the Yocto User Guide - L6.6.36_2.1.0-DOCS or refer to Yoctoproject forum.

 

Regards

Harvey

0 Kudos
Reply

1,099 Views
subbuemdtest
Contributor I
Hi @Harvey021 ,

we are using IMX8qxp-mek board in that we want to enable LVDS-HDMI but during dmesg we are facing probe failed lvds-hdmi channl@0 disabled only we are getting. so can you provide the dtb file which is already enabled the lvds-hdmi bridge connection.

we are not using the official image , we are using custom yocto image.

Thanks,
subbu
0 Kudos
Reply

1,073 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @subbuemdtest 

Would you please raise a new case for enabling LVDS-HDMI for your custom image with more details? 

Sorry, I'm not an expert in this regard. Believe that other engineer will help you.

 

Regards

Harvey

0 Kudos
Reply