Hi,
I am getting occasionally kernels hanging (sometimes hours after boot) with the following output occurring and that just goes on until i reboot the machine:
INFO: rcu_sched self-detected stall on CPU
1-...: (52300 ticks this GP) idle=439/140000000000001/0 softirq=806264/806264 fqs=52291
INFO: rcu_sched detected stalls on CPUs/tasks:
1-...: (52300 ticks this GP) idle=439/140000000000001/0 softirq=806264/806264 fqs=52291
(detected by 0, t=52542 jiffies, g=463552, c=463551, q=391502)
Task dump for CPU 1:
WQ#1(System) R running 4640 28173 28140 0x00000002
Backtrace:
[<beb5bd7c>] (0xbeb5bd7c) from [<beb5bdac>] (0xbeb5bdac)
Backtrace aborted due to bad frame pointer <8007759c>
(t=52545 jiffies g=463552 c=463551 q=391595)
Task dump for CPU 1:
WQ#1(System) R running 4640 28173 28140 0x00000002
Backtrace:
[<80014a38>] (dump_backtrace) from [<80014c80>] (show_stack+0x20/0x24)
r7:807b26c0 r6:60010193 r5:807b26c0 r4:bcfbae00
[<80014c60>] (show_stack) from [<80057204>] (sched_show_task+0xbc/0x118)
[<80057148>] (sched_show_task) from [<80059354>] (dump_cpu_task+0x3c/0x4c)
r5:807b26c0 r4:00000001
[<80059318>] (dump_cpu_task) from [<80082344>] (rcu_dump_cpu_stacks+0x94/0xd8)
r5:807b26c0 r4:00000001
[<800822b0>] (rcu_dump_cpu_stacks) from [<80086698>] (rcu_check_callbacks+0x548/0x860)
r9:bf7d3100 r8:807b26c0 r7:807a460c r6:3f033000 r5:807a4584 r4:807a0100
[<80086150>] (rcu_check_callbacks) from [<8008aca4>] (update_process_times+0x48/0xa8)
r10:8009d204 r9:bf7cfc98 r8:805989c4 r7:00002fd9 r6:bcfbae00 r5:ffffe000
r4:00000000
[<8008ac5c>] (update_process_times) from [<8009d200>] (tick_sched_handle+0x58/0x5c)
r7:00002fd9 r6:23800e91 r5:beb5bde8 r4:bf7cfdb8
[<8009d1a8>] (tick_sched_handle) from [<8009d258>] (tick_sched_timer+0x54/0x9c)
[<8009d204>] (tick_sched_timer) from [<8008b9fc>] (__hrtimer_run_queues+0x160/0x324)
r7:bf7cfc00 r6:beb5a000 r5:00000000 r4:bf7cfdb8
[<8008b89c>] (__hrtimer_run_queues) from [<8008c2e8>] (hrtimer_interrupt+0xc8/0x22c)
r10:bf7cfc78 r9:bf7cfc98 r8:bf7cfc14 r7:00000000 r6:8079cc00 r5:00000003
r4:bf7cfc00
[<8008c220>] (hrtimer_interrupt) from [<80018728>] (twd_handler+0x3c/0x50)
r10:807eea3c r9:f4000100 r8:bf022d80 r7:00000010 r6:bf7d5700 r5:bf08a400
r4:00000001
[<800186ec>] (twd_handler) from [<8007c1e8>] (handle_percpu_devid_irq+0x88/0x1a0)
r5:bf08a400 r4:8079e38c
[<8007c160>] (handle_percpu_devid_irq) from [<8007759c>] (generic_handle_irq+0x30/0x44)
r10:807a4cc0 r9:f4000100 r8:bf034000 r7:00000001 r6:00000000 r5:00000010
r4:8079e38c r3:8007c160
[<8007756c>] (generic_handle_irq) from [<800778a0>] (__handle_domain_irq+0x60/0xc8)
[<80077840>] (__handle_domain_irq) from [<800094c0>] (gic_handle_irq+0x60/0xc4)
r9:f4000100 r8:807eea38 r7:beb5bde8 r6:000003ff r5:000003eb r4:f400010c
[<80009460>] (gic_handle_irq) from [<80593534>] (__irq_svc+0x54/0x70)
Exception stack(0xbeb5bde8 to 0xbeb5be30)
bde0: bf1a1e44 00000000 0000b2cc 0000a7b4 00000000 00000000
be00: ffffffff 01bc9294 bf1a1e40 bf1a1e40 00000001 beb5be44 80592d34 beb5be38
be20: 8009ef44 80592d60 80010013 ffffffff
r10:00000001 r9:bf1a1e40 r8:bf1a1e40 r7:beb5be1c r6:ffffffff r5:80010013
r4:80592d60
[<80592d20>] (_raw_spin_lock) from [<8009ef44>] (futex_wake+0xa4/0x194)
[<8009eea0>] (futex_wake) from [<800a0ec4>] (do_futex+0x128/0xd80)
r10:000000f0 r9:01bc9294 r8:00000001 r7:01bc9294 r6:00000081 r5:00000000
r4:00000000
[<800a0d9c>] (do_futex) from [<800a1ba4>] (SyS_futex+0x88/0x188)
r10:000000f0 r9:beb5a000 r8:80010844 r7:01bc9294 r6:00000081 r5:00000000
r4:00000001
[<800a1b1c>] (SyS_futex) from [<80010660>] (ret_fast_syscall+0x0/0x48)
r10:000000f0 r9:beb5a000 r8:80010844 r7:000000f0 r6:7ee2e842 r5:01bc92b0
r4:00000000
There doesn't appear to be any pattern, when it occurs and I cannot reproduce it. Any ideas on how to debug this issue?
Thanks,
Ivan
Please try the newer release of BSP.
HI,
but there is some similar bug? if yes can you share some details for identify the issue root cause?
Regards,
Ivan