RAW12 support in imx6 MIPI driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAW12 support in imx6 MIPI driver

814 Views
titusstalin
Contributor V

Hello,

Is there any RAW12 with Bayer (BayerRG12) format support in imx6 MIPI driver ?

If not, any reference code or link to implement ?

Regards,

Titus S.

Labels (3)
0 Kudos
Reply
1 Reply

574 Views
b36401
NXP Employee
NXP Employee

Accordingly to chapter 9.2.1.1 "Camera Ports" of i.MX 6D/Q Processor Reference Manual i.MX6 supports up to 16 bits per component Raw (Bayer) image.

Unfortunately we have no sample implementation code for such driver.
Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply