Hi,
I am facing problem in getting proper data from camera (RAW10bit, 2lanes) using MIPI-CSI-0. In each pixel(16bits), 4-MSB bits are getting discarded.
Input & output formats of ISI is set to RAW10
Anyone else is facing the same issue with RAW10 format in imx8qxp? Any lead is appreciated.
Thanks
Statement 1 is right.
-----
MIPI subsystem RAW10 output format is {valid_data, 4’b0} . After right shift 4 bits, you will get the correct image.
-----
There is a mistake in the RM, I´ll ask to fixed. Thanks for the catch.
Regards
Hello, I have the same Problem with an imx8qxp on a ConnectCore8X Board from DIGI Embedded. I do use a Sony IMX327C with 2 lanes over the mipi_csi_0 channel.
In my case i have to set the CHNL_IMG_CTRL[0x04] Register to 0x0f000001 (RAW16 and CSC_BYP enabled) to obtain all bits of the image. When I set it to RAW10 I lose 4 MSBs and when I use RAW12 I lose 2 MSBs. As described above all bits are shiftet 4 bits left. I implemented the 4 bit right shift in software in my demo application. This is very slow but shows the correct image.
For me it looks like the CSI-2 Data formats layer isn't working properly.
My quest now is, how to solve this problem.
Here are my reg dumps with desciption
width=1920, height=1080, fmt.code=0x300f
CSR and HC register dump, mipi csi0
HC num of lanes | [0x100] | 0x00000001 | 2 Lanes |
HC dis lanes | [0x104] | 0x0000000c | Disable Lane 2 + 3 |
HC BIT ERR | [0x108] | 0x00000000 | No Errors |
HC IRQ STATUS | [0x10c] | 0x00000008 | ULPS status change |
HC IRQ MASK | [0x110] | 0x000001FF | All Interrups active |
HC ULPS STATUS | [0x114] | 0x00000000 | No status state active |
HC DPHY ErrSotHS | [0x118] | 0x00000000 | |
HC DPHY ErrSotSync | [0x11c] | 0x00000000 | |
HC DPHY ErrEsc | [0x120] | 0x00000000 | |
HC DPHY ErrSyncEsc | [0x124] | 0x00000000 | |
HC DPHY ErrControl | [0x128] | 0x00000000 | |
HC DISABLE_PAYLOAD | [0x12c] | 0x00000000 | No payload disabled |
HC DISABLE_PAYLOAD | [0x130] | 0x00000000 | No payload disabled |
HC IGNORE_VC | [0x180] | 0x00000000 | Virtual channel active |
HC VID_VC | [0x184] | 0x00000000 | 0 virtual channels expected |
HC FIFO_SEND_LEVEL | [0x188] | 0x00000000 | |
HC VID_VSYNC | [0x18c] | 0x00000000 | |
HC VID_SYNC_FP | [0x190] | 0x00000000 | |
HC VID_HSYNC | [0x194] | 0x00000000 | |
HC VID_HSYNC_BP | [0x198] | 0x00000000 | CSR and HC register dump, mipi csi0 |
CSR PLM_CTRL | [0x000] | 0x00000801 | VALID_OVERRIDE = 1 ENABLE = 1 |
CSR PHY_CTRL | [0x004] | 0x0020007F | RTERM_SEL = 1 S_PRG_RXHS_SETTLE = 7 CONT_CLK_MODE = 1 DDRCLK_EN = 1 AUTO_PD_EN = 1 RX_ENABLE = 1 |
CSR PHY_Status | [0x008] | 0x00000001 | LANES_STOPPED = 1 |
CSR PHY_Test_Status | [0x010] | 0x00000000 | |
CSR PHY_Test_Status | [0x014] | 0x00000000 | |
CSR PHY_Test_Status | [0x018] | 0x00000000 | |
CSR PHY_Test_Status | [0x01c] | 0x00000000 | |
CSR PHY_Test_Status | [0x020] | 0x00000000 | |
CSR VC Interlaced | [0x030] | 0x00000000 | No virtual channel is interlaced |
CSR Data Type Dis | [0x038] | 0x00000000 | |
CSR 420 1st type | [0x040] | 0x00000000 | |
CSR Ctr_Ck_Rst_Ctr | [0x044] | 0x00000001 | CTL_CLK_OFF = 1 |
CSR Stream Fencing | [0x048] | 0x00000000 | No virtual channel is fenced (RW - to Pixelformater) |
CSR Stream Fencing | [0x04c] | 0x00000000 | No virtual channel is fenced (RO - from Pixelformater) |
CHNL_CTRL | [0x00] | 0xE0FF0002 | CHNL_EN = 1 CLK_EN = 1 CHNL_BYPASS = 1 SEC_LB_src=0 src=2 (MIPI) |
CHNL_IMG_CTRL | [0x04] | 0x0F000001 | FORMAT = RAW16 GBL_ALPHA_VAL = 0 GBL_ALPHA_EN = 0 DEINT = 0 DEC_X = 0 DEC_Y = 0 CROP_EN = 0 VFLIP_EN = 0 HFLIP_EN = 0 YCBCR_MODE = 0 CSC_MODE = 0 CSC_BYP = 1 |
CHNL_OUT_BUF_CTRL | [0x08] | 0x00000092 | LOAD_BUF1_ADDR = 0 LOAD_BUF2_ADDR = 0 PANIC_SET_THD_Y = PANIC > 12,5% OUT BUF |
CHNL_IMG_CFG | [0x0c] | 0x04380780 | HEIGHT = 1080 WIDTH = 1920 |
CHNL_IER | [0x10] | 0x3DFF0000 | FRM_RCVD_EN = 1 AXI_WR_ERR_V_EN = 1 ... ALL IRQs EN = 1 |
CHNL_STS | [0x14] | 0x00000200 | LINE_STRD = 0 FRM_STRD = 0, AXI_WR_ERR_U = 0 ... PANIC_V_BUF = 0 OFLW_V_BUF = 0 ... BUF1_ACTIVE = 1 BUF2_ACTIVE = 1 |
CHNL_SCL_IMG_CFG | [0x98] | 0x04380780 | HEIGHT = 1080 WIDTH = 1920 |
CHNL_SCALE_FACTOR | [0x18] | 0x10001000 | Y_SCALE = 1.0 X_SCALE = 1.0 |
CHNL_SCALE_OFFSET | [0x1c] | 0x00000000 | Y_OFFSET = 0.0 X_OFFSET = 0.0 |
CHNL_CROP_ULC | [0x20] | 0x00000000 | X = 0 Y = 0 |
CHNL_CROP_LRC | [0x24] | 0x00000000 | X = 0 Y = 0 |
CHNL_CSC_COEFF0 | [0x28] [0x2c] [0x30] [0x34] [0x38] [0x3c] | 0x00000000 | |
CHNL_ROI_0_ALPHA | [0x40] | 0x00000000 | ALPHA = 0 ALPHA_EN = 0 |
CHNL_ROI_0_ULC CHNL_ROI_0_LRC | [0x44] | 0x00000000 | X = 0 Y = 0 |
... | |||
CHNL_OUT_BUF1_ADDR_Y | [0x70] | 0xA7000000 | |
CHNL_OUT_BUF1_ADDR_U | [0x74] | 0x00000000 | Not used in one plane operation |
CHNL_OUT_BUF1_ADDR_V | [0x78] | 0x00000000 | Not used in one or two plane operation |
CHNL_OUT_BUF2_ADDR_Y | [0x8c] | 0xA6400000 | |
CHNL_OUT_BUF2_ADDR_U | [0x90] | 0x00000000 | Not used in one plane operation |
CHNL_OUT_BUF2_ADDR_V | [0x94] | 0x00000000 | Not used in one or two plane operation |
CHNL_OUT_BUF_PITCH | [0x7c] | 0x00000F00 | LINE_PITCH = 3840 |
CHNL_IN_BUF_ADDR | [0x80] | 0x00000000 | RESERVED |
CHNL_IN_BUF_PITCH | [0x84] | 0x00000000 | RESERVED |
CHNL_MEM_RD_CTRL | [0x88] | 0x00000000 | RESERVED |
Hi,
I am using RGB888 format, Image is displaying in HDMI port but strips are adding in image, I am thinking some bits are missing. Please help us to resolve this Issue. I am getting Image as below.
Thanks & Regards,
Mallikarjuna B.
@Bio_TICFSL
I am experiencing the same issue
Do you have any update on this issue with the CSI-2 data formats layer?
Hi pmliquify,
I am trying to stream Monochrome camera Y10 in imx8qm facing the same issue like you. The Y10 data is left shifted by 4. did you had any solution for this?
Please help me if you have any.
Thanks and regards
I think there is some confusion in the TRM(REV-E): i.MX 8DualX/8DualXPlus/8QuadXPlus Applications Processor Reference Manual
Statement 1:
The CSI data is right LSB aligned and zero padded depending
on data format. When interfacing ISI, CSI data is shifted 6-bits
due to ISI bits [5:0] always being zero
(0bxxCSIDATAxxxxxx). All RAW14, RAW12, RAW10,
RAW8, and RAW6 video data is filled from BIT[13] to LSB,
the remaining bits are zero padded. Only RAW16 input data
will be saved to memory from BIT[15] to LSB.
Statement 2:
001100b - RAW10 - 10-bit RAW data packed into 16-bit WORD with 6 LSBs waste bits
Found that statement 1 doesn't matches with statement 2.
Hello wasim,
Supported cameras and formats are described in AN12187 Quick Start Guide
for MINISASTOCSI for i.MX 8M Evaluation Kit
https://www.nxp.com/docs/en/application-note/AN12187.pdf
It support raw10, t1he clocks are MIPI CSI host clocks, they are not related to external camera input signal.
The host can support 1, 2,3 and 4 lanes camera, so 1 lane camera can be supported. The lane number is set from device tree, "data-lanes = <1 2>;" means 2 lanes are used:
&mipi_csi_1 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
port {
mipi1_sensor_ep: endpoint1 {
remote-endpoint = <&ov5640_mipi1_ep>;
data-lanes = <1 2>;
};
csi1_mipi_ep: endpoint2 {
remote-endpoint = <&csi1_ep>;
};
};
};
Hi BioTICFSL,
Thanks for your reply.
Our SOC is 8QXP MEK and not 8M.
I have tried for both single lane and multi-lane. Our endpoint supports 2 lanes.
Any idea on the documentation of CSI2 Subsystem CSR registers.
Thanks
We tried using single data-lane but still the same issue.
Can anyone help?