RAM part number is same but SOM part number is different

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RAM part number is same but SOM part number is different

1,410 次查看
shamiullah
Contributor III

Hello everyone,

I am using two different boards. One is NXP board and and the other is customized board but the processor part number is different. MIMX8MM3DVTLZAA and MIMX8MM5DVTLZDA are the two different boards SOM part numbers but they use the same RAM part number MT53D512M32D2DS-053 WT:D . Are they any changes we have to make two configure same part number RAM on other board? We are having the RAM configuration data of EVK but can we use the same thing in other customized EVK with same RAM part number  but different SOM part number?

Please let me know if any ..... Thanks in advance

标签 (1)
0 项奖励
回复
4 回复数

1,401 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi shamiullah,

 

These processors are pin to pin compatible, so you should not have problems selecting the DDR or other processor, also check with the owner of the customized EVK to see if they don't have problems by doing this, but as I said, you should not have problems with this.

 

Hope this helps you.

Regards,

Israel.

0 项奖励
回复

1,383 次查看
shamiullah
Contributor III

 .

0 项奖励
回复

1,391 次查看
shamiullah
Contributor III

Hi nxf63675,

Can i confirm from your information that i can use the same DCD table files in uboot for both the processors?

Thanks & Regards

Shamiullah

0 项奖励
回复

1,349 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi shamiullah,


Well, yes but you will need to use the BSP from the customized board as our BSP is for ours EVK's, If for some reason you have problems booting up you could use the DDR tool to generate a new DCD table, please see the next link:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

 

Hope this helps you.

Regards,

Israel.

0 项奖励
回复