Hi all,
I'm building the imx6sabresd machine with the Linux 4.1.15_1.2.0 BSP. Unfortunately, the network access to freescale/NXP servers (git://git.freescale.com) is erratic : I had to re-run several times the build (bitbake core-image-minimal) when it comes to fetch u-boot. So I'm trying to understand the download (fetch) system.
When it fails, we can see this in the corresponding log.do_fetch file :
DEBUG: Trying PREMIRRORS [...] DEBUG: For url git://git.freescale.com/imx/uboot-imx.git;protocol=git;branch=imx_v2015.04_4.1.15_1.0.0_ga returning http://downloads.yoctoproject.org/mirror/sources/git2_git.freescale.com.imx.uboot-imx.git.tar.gz [...] DEBUG: Fetcher failure: Fetch command failed with exit code 8, output: http://downloads.yoctoproject.org/mirror/sources/git2_git.freescale.com.imx.uboot-imx.git.tar.gz: 2017-02-23 12:00:25 ERROR 404: Not Found. [...] DEBUG: Trying Upstream DEBUG: Fetcher failure: Fetch command failed with exit code 128, output: Cloning into bare repository '/home/yon/fsl-nxp-1.2.0/downloads//git2/git.freescale.com.imx.uboot-imx.git'... fatal: read error: Connection reset by peer [...] DEBUG: Trying MIRRORS [...] DEBUG: Fetcher failure: Fetch command failed with exit code 8, output: http://sources.openembedded.org/git2_git.freescale.com.imx.uboot-imx.git.tar.gz: 2017-02-23 12:00:29 ERROR 404: Not Found. ERROR: Fetcher failure: Fetch command failed with exit code 128, output: Cloning into bare repository '/home/yon/fsl-nxp-1.2.0/downloads//git2/git.freescale.com.imx.uboot-imx.git'... fatal: read error: Connection reset by peer DEBUG: Python function base_do_fetch finished DEBUG: Python function do_fetch finished ERROR: Function failed: Fetcher failure for URL: 'git://git.freescale.com/imx/uboot-imx.git;protocol=git;branch=imx_v2015.04_4.1.15_1.0.0_ga'. Unable to fetch URL from any source.
Thanks in advance for your help,
-Yvon
解決済! 解決策の投稿を見る。
Hello Yvon,
The NXP git does allow to download specific branches or commits
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/
The mirrors may not offer all alternatives and are sometimes impractical as they may contain compressed files etc. I’m not sure if there is a unified practice in regards of how mirrors are offered.
You may be able to disable mirrors by setting the variables MIRRORS/PREMIRRORS to an empty string on local.conf although I haven’t tried this. I’m also trying to sort out how mirrors and premirrors are handled in terms of priorities.
A good option when working with a not so stable connection or when you would like to work offline at some point is to fetch the required sources for a specific image or package and building at a later time. You can do this by running:
$ bitbake <image_or_recipe> -c fetchall
I know this is a workaround, but it may be helpful in some scenarios and it’s easier than cloning the repositories and then changing SRC_URI to the local clone.
I hope this information helps! My apologies for the inconvenience.
Regards,
Hello Yvon,
The NXP git does allow to download specific branches or commits
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/
The mirrors may not offer all alternatives and are sometimes impractical as they may contain compressed files etc. I’m not sure if there is a unified practice in regards of how mirrors are offered.
You may be able to disable mirrors by setting the variables MIRRORS/PREMIRRORS to an empty string on local.conf although I haven’t tried this. I’m also trying to sort out how mirrors and premirrors are handled in terms of priorities.
A good option when working with a not so stable connection or when you would like to work offline at some point is to fetch the required sources for a specific image or package and building at a later time. You can do this by running:
$ bitbake <image_or_recipe> -c fetchall
I know this is a workaround, but it may be helpful in some scenarios and it’s easier than cloning the repositories and then changing SRC_URI to the local clone.
I hope this information helps! My apologies for the inconvenience.
Regards,