Hi steven
usage of these pins are programmable, please look at sect.
25.2.2 Serial Transmit 1 Data Pin i.MX6DQ Reference Manual :
TX1 is used for transmitting data from the ESAI_TX1 serial transmit shift register.
from sect.25.2.3 Serial Transmit 2/Receive 3 Data Pin :
TX2_RX3 is used as the TX2 for transmitting data from the ESAI_TX2 serial transmit
shift register when programmed as a transmitter pin..
TX2_RX3 is an input when data is being received by the ESAI_RX3 shift register.
sect.25.6.14 Transmit Control Register (ESAI_TCR), ESAI_TCR bits TEn
enable the transfer of data from ESAI_TXn
http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------