Dear, all
I'd like to know below camera specifications for i.MX8M
1) What's the maximum camera supported resolution for snapshot (still shot)?
For example) jpeg, 2592x1944
As far as I know, ov5640 (it's mounted on i.MX8M Evk) support 5MP resolution. Does i.MX8M also support the maximum resolution of the camera sensor?
2) What's maximum video recording resolution/frame rate?
As I know i.MX8M support 1080p/30fps and H.264 S/W encoder only. Is it the same as the camera preview usecase?
Thanks you.
Dear Rita,
Thanks for answering all my questions!
It's my pleasure. If you have new questions you can create new threads and contact us.
Have a nice day
Rita
2) There is no maximum video recording resolution/frame rate in software. They are not the same. The maximum video recording resolution/frame rate is depending on your using.
Hi,
1)Yes,You are right. The maximum resolution is 2592x1944. Details you can see the document https://www.nxp.com/doc/AN12187 .
Have a great day,
Rita
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------