Questions about System calibration template of surround view application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about System calibration template of surround view application

602 Views
Jay_Jiang
Contributor I

Hi,

In “Surround View Application Reference Manual ”, "4.2 System calibration template", Figure 13 shows  Extrinsic camera parameters’ calibration pattern. From this figure,  it seems that the "Poster Height "  could be different from the "Poster Width". If so, the calibration pattern would be a rectangle. 

However, from the source code of SVA, seems that SVA requires the calibration pattern be square( with equal poster height and width).

So my question is, 

Can the  Extrinsic camera parameters’ calibration pattern poster be rectangle,

or it has to be square?

 

Regards,

Jay

 

 

 

0 Kudos
Reply
1 Reply

567 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @Jay_Jiang 

The calibration pattern can be a rectangle, it is not limited to square.

B.R

0 Kudos
Reply