Questions about PMU of i.MX28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about PMU of i.MX28

Jump to solution
697 Views
hikaruuruno
Contributor III

Hello all,

Recently we made a custom board with i.MX280 on it which is VDD5V source only configuration.

When 5V is supplied to i.MX280 without any boot devices, VDDIO_3V3, VDDA_1V8 and VDDD becomes likely voltages.

(VDDIO_3V3 : ca. 3.15V / VDDA_1V8 : ca. 1.79V / VDDD : ca. 1.18V)

But VDD4P2 and VDD1P5 become weird value. VDD4P2 becomes ca. 0.8V and VDD1P5 0V.

i.MX280_Power.png

I suppose the voltage of VDD4P2 is not really weird since there is no boot devices and the LinReg is not enabled yet.

But according to the Figure 1 of AN4199, LinRegs of VDD1P5 and VDDD is supplied by LinReg of VDDA.

So if LinReg of VDDD is working, LinReg of VDD1P5 should be working, too.

It does not really matter because we do not use 1.5V, but the behavior seems too creepy.

Does anyone know what's going on in the chip, or it causes any problem or not?

By the way, we are considering to change the configuration to DCDC_BATT source only to reduce the power consumption.

In case of DCDC_BATT source only configuration, can we remove the 33uF capacitor(s) and 0.1ohm resistors connected to VDD4P2? (C5 to C7, C185, C191 and R363, R364 of the evk_revD schematics.)

Since these capacitors and resistors take too much space, we want to remove them.

If we cannot remove these, does anyone can tell us how much watts the 0.1ohm should allow?

We would like to minimize the size of Rs.

Thank you in advance,

Hikaru

Labels (1)
0 Kudos
Reply
1 Solution
503 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hikaru

VDD1P5, VDD4P2 by default are disabled, can be turned on

by software. If VDD4P2 is not used, capacitor(s) and resistors connected to

it can be removed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
504 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hikaru

VDD1P5, VDD4P2 by default are disabled, can be turned on

by software. If VDD4P2 is not used, capacitor(s) and resistors connected to

it can be removed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply