Questions about HDMI ARC in MCIMX8M-EVK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about HDMI ARC in MCIMX8M-EVK?

Jump to solution
2,049 Views
js8084
Contributor I

Hi

I'd like to record the TV Audio which is connected through HDMI-ARC. (TV will send the audio through HDMI-ARC). 

In the datasheet of i.MX8 Processors, it says that supports HDMI-ARC(Audio Return Channel). I'm wonder whether MCIMX8M-EVK supports HDMI-ARC path and I can receive the audio data in Linux

Thank you very much

 

 

 

0 Kudos
Reply
1 Solution
2,015 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi js8084,

>>Is this also possible to capture the raw data(=encoded data, not decoded PCM) that is transmitted from TV through HDMI-PCM? 

Below is from i.MX Expert:

----------------------------------------

This requirement needs to enhance the HDMI CEC command.  It means you need to let the TV know that the board support compressed streams by CEC command.  then TV will send the encoded data to board.

----------------------

Have a nice day!

B.R,

weidong

View solution in original post

0 Kudos
Reply
3 Replies
2,016 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi js8084,

>>Is this also possible to capture the raw data(=encoded data, not decoded PCM) that is transmitted from TV through HDMI-PCM? 

Below is from i.MX Expert:

----------------------------------------

This requirement needs to enhance the HDMI CEC command.  It means you need to let the TV know that the board support compressed streams by CEC command.  then TV will send the encoded data to board.

----------------------

Have a nice day!

B.R,

weidong

0 Kudos
Reply
2,044 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

   >> I'm wonder whether MCIMX8M-EVK supports HDMI-ARC path and I can receive the audio data in Linux

   Yes, right.

    You can find the device, and use arecord to test it.

 

Have a  nice day!

B.R,

weidong

0 Kudos
Reply
2,040 Views
js8084
Contributor I

Thank you very much.

If you don't mind, I have another question.

Is this also possible to capture the raw data(=encoded data, not decoded PCM) that is transmitted from TV through HDMI-PCM? 

Best Regards,

JS

 

 

 

0 Kudos
Reply