Hello,
I think the recommendations in the following Community thread may be also
applied for this case.
SDRAM configuration of iMX6DL / Sabre
When considering the timing values, DDR3-800 should be taken, assuming 400 MHz as
working frequency. General idea is to use more safe (relax) values.
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.