Question on IMX6QP Camera Input Capability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question on IMX6QP Camera Input Capability

1,191 次查看
davidtrinh
Contributor II

Hi Community,

I have a question to ask regarding the data throughput of the IMX6QP camera interface.

I have a hardware setup as follow:

1 (ONE) 3.2MP@38fps YUV422 camera connect to the IMX6QP MIPI-CS2 4 lanes port.

2 (TWO)  HD 1280x720@30fps YUV422 cameras connect to each of the IMX6QP VIN (Parallel) ports

Our design target is for this setting to work in the way that the IMX6QP will read all these 3 camera simultaneously without frame drop. I have checked the Reference manual and related application notes. All in all, I am understanding that the IMX6QP can handle this setting seamlessly.

(My board has 64-bit DDR3 setting)

My question is : is my above assumption correct?! If not, what is the problem here?

Thank you for you time to my question.

Cheers, 

David

标签 (1)
0 项奖励
回复
2 回复数

1,107 次查看
igorpadykov
NXP Employee
NXP Employee

Hi David

you are right. all these cameras can be supported by i.MX6QP.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,106 次查看
davidtrinh
Contributor II

Dear Igorpadykov,

Thanks for your reply. Highly appreciate your time.

Cheers,

David

0 项奖励
回复