Hi Miyamoto
>1. Are there any time specific regulations on power-on or power-down sequence?
no
>2. Is it possible for NVCC_XXX or NVCC_DRAM to rise up during VDDA_1P8_XXX or VDDA_DRAM are rising-up?
no
>Or should those (NVCC_XXX or NVCC_DRAM) rise-up after the completion of VDDA_1P8_XXX or VDDA_DRAM >rising-up?
according to sect.3.2.1 Power-up sequence i.MX8M Datasheet steps should be
• Turn on VDDA_1P8_XXX, VDDA_DRAM (no sequence between these rails)
then
• Turn on NVCC_XXX and NVCC_DRAM (no sequence between these rails)
>3.exact meaning of “power-up”.
it is power-up sequence defined in sect.3.2.1 Power-up sequence i.MX8M Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX8MDQLQCEC.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------