Question: i.MX8M Mini possible to generate MCLK while in I2S slave mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question: i.MX8M Mini possible to generate MCLK while in I2S slave mode?

1,064 Views
sagisaka
Contributor I

Hello,

I'm quite newbie to i.MX series and now designing custom board with design partner.

OS works on it will be a customized embedded linux.

I'd like to interface i.MX8M Mini (hereinafter called just SoC) with certain DSP that needs external MCLK while it's in I2S master mode.

Originally, MCLK (24.576MHz) is generated by clock device aside from DSP and SoC, but now we're trying to remove it for cost, by generating MCLK from SoC.

One concern is, even SoC needs to be a I2S slave, if it's possible to generate MCLK or not.

If not, then alternatively generate MCLK from another SAI is possible or not?

Thanks,

Kind regards,

Takashi

0 Kudos
Reply
2 Replies

1,021 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

>even SoC needs to be a I2S slave, if it's possible to generate MCLK or not.

yes possible.

>alternatively generate MCLK from another SAI is possible or not?

yes possible.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,021 Views
sagisaka
Contributor I

igorpadykov

Thank you for your fast response.

Let me try and if we have difficulty let me ask question again (maybe in the domain of register configuration, Linux device driver configuration).

Kind regards,

Takashi

0 Kudos
Reply