Hi team,
My customer is considering the use of following Micron/NAND flash chip with i.MX6UltraLite.
NAND512W3A2SN6E or MT29F1G08ABAEAWP-IT:E or MT29F2G08ABAFAWP-IT:F
Or MT29F32G08CBADBWPR:D
I think all those chips can be used for i.MX6UltraLite, according to its reference manual.
Could you please double-check that those NAND chips, as a boot device or a storage device, can be used with i.MX6UL?
Please find the attached files for the datasheet.
Thanks,
Miyamoto
Original Attachment has been moved to: NAND.zip
Hello,
The mentioned NANDs may be used with i.MX6UL.
In particular, according to section 8.5 [Boot Devices (Internal Boot)] of the i.MX6UL RM :
"Raw NAND (MLC and SLC), and Toggle-mode NAND flash through GPMI-2
interface. Page sizes of 2 Kbyte, 4 Kbyte and 8 Kbyte. Bus widths of 8-bit with 2
through 40-bit BCH Hardware ECC (Error Correction) are supported."
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------